Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
batterymgmt-Pt1-slide14

Finally, this slide shows that charging a cell too fast can degrade its performance over time. For a 900 mAH rated battery, the “C” rate is 900mA. In particular, for most Li-Ion batteries, it is recommended to recharge slightly lower than the “1C” rate, so the overall charge time may be in the 90 minutes to two hours range. However, some new cell types are optimized for high power applications, and allow high rate charging, so this data may not apply to all battery types.

PTM Veröffentlicht am: