Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
batterymgmt-Pt1-slide10

This chart shows the discharge of the same type of cell in the previous chart at a fixed current, but for different temperatures. Because the internal resistance is lower at high temperatures, the high temp curves have higher output voltage than the low temp curves. The same self-heating can be seen in the cold temperature examples near the beginning of the discharge cycle.

PTM Veröffentlicht am: