Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
EZA-Slide8

Up to eight units can be paralleled in droop mode current share mode for larger systems using the RS-485 interface. The units are fully isolated from input to output and to ground. As previously mentioned, the RS-485 can be used to set the operating mode depending on the application and the needs of the user.

PTM Veröffentlicht am: