Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Thermal Interface Product Selection Slide 19

The next critical parameter to consider is electrical isolation. The only truly conductive TIMs are those based on graphite. Gap fillers based on silicone or non-silicone are generally considered to be electrically isolating. PCMs and greases, however, are not rated as either conductors or insulators. If applied thick enough, they can provide some degree of isolation; although, if voids are present in the material they could provide a route for short circuits, possibly causing catastrophic component failure.

PTM Veröffentlicht am: