Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Thermal Interface Product Selection Slide 13

It is also of critical importance to consider how the joint is clamped, as this will influence the maximum and minimum gap. It is essential that an appropriate thickness of gap filler is selected so that the material is always under an appropriate level of compression. As a general rule of thumb, a gap filler should always be used under a compression of 20 – 45%. To ensure a constant and even pressure in high power dissipation applications, spring clips or fasteners are preferred.

PTM Veröffentlicht am: