Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
Thermal Interface Product Selection Slide 12

There are a number of key design criteria to consider when selecting a TIM for a specific application. Firstly, it is important to consider the amount of heat that needs to be dissipated. If there is a large amount of heat to dissipate, low thermal resistance products, such as thermal greases or PCMs, would be a much better choice. It is also important to consider the clamping pressure the TIM will be put under as this will determine the thermal resistance of the product, greatly impacting the selection of the material.

PTM Veröffentlicht am: