Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
BiCMOS to the Latest RF Product Family Slide 17

One of the areas this presentation focused on is RF synthesizers; they are used in a wide variety of applications and are important in a variety of radio units. ST has a full range of RF synthesizers for creating devices from the ones aimed at base stations, which range from 625 MHz to 5 GHz bands up to the future STuW81300 device, to be introduced mid-year 2015, which covers up to 16 GHz. Developments such as this are an area to which ST is devoting a lot of manpower, resources, and technology.

PTM Veröffentlicht am: