Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
BiCMOS to the Latest RF Product Family Slide 13

As was previously mentioned, more than one STW8110x device covers this band. It is a family of devices that is needed to cover the band that is being looked at, from 625 MHz up to 5 GHz. Depending upon the customer’s needs it could be convenient if they are just interested in a smaller band and it fits in one of the bands shown on this slide. With the STW8110x family of devices evaluation boards, evaluation kits, software GUIs for programming, and a PLL simulation tool are available.

PTM Veröffentlicht am: