Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Product List
PMIC: CP240x LCD Driver Family Slide 9
For the LCD to operate correctly and to preserve the life of the display the voltage to the segments needs to be AC with a 0 V DC component. The LCD controller generates the waveforms used to drive the segments of the display. The output voltage is the difference between the common waveform and the intermediate segment waveform. In the example above, the “ON” condition is shown and is the result of subtracting the segment waveform from the common waveform which produces a 0V DC biased AC waveform.
PTM Veröffentlicht am: