Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Product List
Input Capture/Output Compare

An add-on circuit to the timer is the capture/compare module. This provides the capability to store the timer value when an external event occurs during capture mode. In the compare mode, an output flag from the timer module identifies when a match occurs between a value stored in an SFR and the timer count value using a comparator. There are many different uses for these types of events, however, in the CP240x devices this method can be used to calibrate the smaRTClock oscillator with the system clock. In the examples provided, the capture event stores the value of the timer in the capture register and the compare event occurs when the timer value matches the value stored in the comparator.
PTM Veröffentlicht am: