Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Pull-Up Resistors (cont’d.) Nexperia's LSF Scenario 2

The pull-up resistor value can also be calculated from the scenario where the B-side is driving a low level. Just like the previous calculation, the pass transistor is on so current is flowing from the B-side to the A-side. Again, the RPU is normally the same on both sides and the RDS(on) of the pass transistor can be neglected. By using the same equations as the previous page, the same pull-up resistor value can be calculated. Remember that for high-level drive from either side, the pass transistor is not conducting so the performance of the A and B sides are solely based on the value of the pull-up resistors. This is the reason that the lowest value pull-up resistor will result in the sharpest rising edge on both sides.

PTM Veröffentlicht am: