Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
NMUSB202MC-Slide3

The simplest hubs available on the market are not without their shortcomings as many do not have isolation – the upstream circuitry ground connects through to the downstream circuitry ground. The power available from the downstream ports may be limited, typically only 100mA each. This can limit a user application which requires greater power and poses potential operational issues.

PTM Veröffentlicht am: