Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
EEPROMs-Slide10

This plug-and-play device also comes with additional EEPROM capability to help store configuration settings or lookup tables or buffer small amounts of data. These chips are available in SPI, I²C and the UNI/O® bus to offer designers the flexibility to select the one that best fits into an application. Also note that the actual EUI-48™ node address is stored in the last 6 bytes of the memory array with the Most Significant Bit in the lowest memory address or the Big Endian convention.

PTM Veröffentlicht am: