Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
PIC24FJDA-Slide20

To provide developers with a low cost development environment, Microchip offers the PIC24FJ DA graphics development board. The Microchip display connector on the board provides the flexibility to either use the available TFT LCDs from Microchip or a display of the developer’s choice. Additionally, the board features capacitive touch pads, USB host and device connectors, PICtail Plus daughter board expansion slot and program/debugging interface.

PTM Veröffentlicht am: