Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
surge-protection-slide8

Why use an LED surge protection module? The major purpose of installing and using LED lighting is to save energy. But, customers will not obtain the full value proposition of LED lighting energy savings if the luminaire gets damaged due to a transient surge during its lifetime. The LSP05 and LSP10 modules value proposition is protecting the LED lighting fixture investment and also indicating when module replacement or lighting recover is needed. Therefore, using these modules minimize overall maintenance costs. 

PTM Veröffentlicht am: