Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Slide8

The most common application for RF Synthesizers / PLLs is as a local oscillator in wireless base station radio cards. The device is used to provide a reference frequency to the mixer, modulator or demodulator in order to modulate the signal from RF to an intermediate frequency (IF) or baseband frequency, or to modulate the signal from a baseband frequency to an IF or RF frequency. Renesas also offers a very large selection of extremely high performance RF devices including these mixers, modulator or demodulators.

PTM Veröffentlicht am: