Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
Slide6

Displayed here is another example of a phase noise plot taken this time at a much higher frequency (3500 MHz). The phase noise performance is again very good (better than similar devices from other manufacturers) and the spurious power level remains below -80 dB. Of course, the actual phase noise numbers follow the Leeson’s principle and therefore differ from the numbers on the previous slide as they scale to a higher frequency.

PTM Veröffentlicht am: