Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
POL-Slide13
OmniOn Power is the inventor of the tunable loop feature that offers the best performance at the lowest cost. Tunable loop is a feature that allows the user to add small external components to the existing pins of a module in order to adjust the compensation characteristics of the module. This means that the same module can be used in applications with high transient requirements as well as under more benign conditions. This also allows the user to use the lowest number of external capacitors, a feature that allows for cost and space reductions while enhancing reliability.
PTM Veröffentlicht am: