Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
multiple
NXP developed a benchmark test and used it to compare the MC9S08LL64/16 to a well known LCD microcontroller competitor that will be referred to as “Competitor A”. The 9S08LL16 and 9S08LL64 devices provided up to 76% improvement when the conditions shown on this slide are placed on the microcontrollers. NXP LCD MCUs have such a power consumption advantage because of their multiple power saving modes, independent clock gating for all peripherals, functionality of peripherals in low power, and bus clock/flash programming functionality.
PTM Veröffentlicht am: