Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
SAW-Slide6

A structure called an Interdigital Transducer (IDT), with alternate positive and negative electrodes, is implemented on the surface of the quartz substrate so that a wave-like vibration is emitted across the surface. The oscillation frequency is inherent in interval between the electrodes (  ) and the propagation speed of sound (V) within the substrate. This type of quartz cut and structure is able to produce much higher frequencies than a tuning fork crystal or AT cut crystal. Like all of Epson’s timing and sensor products, a quartz substrate is used for its piezo-electric property, high reliability and stable characteristics over temperature.

PTM Veröffentlicht am: