Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
SBR-Slide8

With a lower coefficient of leakage over temperature, the SBR technology also has a much higher thermal runaway temperature than a Schottky rectifier. When tested without a heatsink, the SBR has a thermal runaway temperature of 185C compared to the Schottky thermal runaway temperature of 130C. When operated with a heatsink, this difference is even larger resulting in greater stability and higher operating temperatures.

PTM Veröffentlicht am: