Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
SBR-Slide2

The performance and reliability of power diodes are often limited by their design. Schottky rectifiers are the dominant technology in this area for rated voltages below 200 V. Schottky rectifiers use a metal-semiconductor contact which limits their stability at high temperatures and greatly reduces their reliability over time. The Super Barrier Rectifier (SBR) technology overcomes these issues by using a CMOS ion implantation process which allows for flexibility in the control of the VF/IR trade-offs and increased reliability.

PTM Veröffentlicht am: