Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
prototype Cypress demo video
Once the user is familiar with the configuration of the capacitive button parameters using EZ-click, they can easily prototype their solution using the CY3280-MBR3 evaluation kit. The steps are: connect the CY8C3280-MBR3 evaluation kit to the PC; open the EZ-Click software to configure capacitive button parameters; assign the LED control signals to turn the button LEDs ON or OFF; test SmartSense auto-tuning performance by varying the parasitic capacitance and overlay thickness; and prototype the design using the expansion connectors. It is recommended that the designer also watches the demo video.
PTM Veröffentlicht am: