Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
terms used
The next two slides highlight a few specific terms that will be used in this presentation. CapSense is Cypress’s solution for capacitive buttons. Capacitive buttons parameters are stored as register data that controls the configuration, operation, and performance of MBR capacitive buttons. Manual tuning is the manual process of configuring capacitive button parameters for optimal performance. It is required to compensate for system, manufacturing, and environmental changes. SmartSense auto-tuning is a CapSense algorithm that automatically configures capacitive button parameters for optimal performance. It continuously compensates for any system, manufacturing, and environmental changes. Register-configurable solution is a CapSense solution that can implement specific features by configuring capacitive button parameters without the need for firmware development.
PTM Veröffentlicht am: