Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Switch Fundamentals Slide 21

Transition time is the time required to switch from one channel to another channel. The enable/disable time is the time required for a MUX to connect/disconnect output from selected input. The time delay added to an input signal by the switch channel, when a signal is passing through the channel, is the Propagation Delay.

PTM Veröffentlicht am: