Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
Switch Fundamentals Slide 13

Capacitance is another important parameter to consider in any design, and therefore, the following parameters are specified in the datasheet: CS(off) is the source off capacitance and is measured between the source input and GND when the switch is off or disabled; CD(off) is the drain off capacitance and is measured between the drain output and GND when the switch is disabled; CS(on) is the on switch capacitance and is measured between the input or output and GND; On capacitance is a measure of the source capacitance, drain capacitance and the switch capacitance for an on switch; and C(in) is the digital input capacitance and is measured between the digital input and GND.

PTM Veröffentlicht am: