Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
PoweringFPGA-Slide9

The alternative to a CPA is the distributed power architecture, DPA. With the DPA a single, semi-regulated DC voltage is distributed throughout the system and individual DC/DC converters (linear or switching) are located adjacent to each load. The distance between the DC/DC converter and the load, e.g. FPGA, is much shorter with a DPA which reduces the voltage decrease from line resistance and the voltage dip from wiring inductance. This method of local powering of loads is named point-of-load, POL.

PTM Veröffentlicht am: