Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
MEG-Array Mezzanine Connectors Slide 10

Ball Grid Array technology has many advantages, including lower production cost when compared to press fit terminations. The ability to use reflow processing allows termination of the connector simultaneously with other surface mount components. BGA termination also helps in high speed applications since vias can be eliminated or minimized. Routing becomes easier due to minimal vias, and double sided connectorization is possible since there are no parts of the connector protruding through the board.

PTM Veröffentlicht am: