Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
HSHM-Slide3

There are three common problem situations. The first is the 2mm HM backplane connectors used in legacy VERSAmodule Eurocard (VME) systems. The industry standard connector designated ‘P0’ (also known as the ‘B19’) on VME64x with VITA31 is limited to a maximum speed of 1.5Gbps per differential pair. VXS standard allows faster (5Gbps) speeds but the 7-row VXS connectors are not compatible with VITA31.

PTM Veröffentlicht am: