Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
Application Benefits

All of the application benefits tie back to the VCSEL as the emitter. The maximum sensing range using a mirror is four times greater than the VCNT2025X01 and seven times greater than the VCNT2020. Because it has a ±11o emission angle, the window diameter can be half the size. Finally, the mechanical placement of the VCNT2030 behind the cover or window is between 0 and 2 mm, more flexible from a manufacturing standpoint.

PTM Veröffentlicht am: