Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
Phototriac Slide 2

Optocouplers transmit a signal while electrically isolating the transmitting and receiving sides. They play a key role in protecting sensitive electronics and the consumer from high voltage spikes. A current turns on the infrared emitting diode, the infrared light from the IRED travels through the transparent dielectric material to a photo detector. The photo detector generates current which is then used to perform various functions. The dielectric allows light to pass but blocks electrical noise and voltage spikes.

PTM Veröffentlicht am: