Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
fusing
The series has well-established interruption behavior as function of the overload power applied for resistance range < 560 Ω, as shown on the graphs here. This series can be used as a fusible resistor with defined fusing time for resistances from 0.22 Ω to 560 Ω for the PR01, 0.33 Ω to 560 Ω for the PR02 and 0.68 Ω to 560 Ω for the PR03.
PTM Veröffentlicht am: