Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Slotted Switches Slide 8

When selecting the proper device, first make sure the object blocking the light will easily fit into the slot. Next, determine how accurately you need to identify the location of the object passing through the slot. Is this a clean or dusty environment? What are the temperature extremes? What kind of other contaminations are around? What type of electrical interface do you need? Will the sensor provide an Ic (on) current that can be used to accurately identify the location of the object? Photo darlingtons provide high gain while Photologic devices provide logical output states and high speed switching.

PTM Veröffentlicht am: