Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
PandaBoard Overview Slide 3
Providing new application possibilities, PandaBoard comes with the ability to drive two independent displays simultaneously: one via an HDMI port and another via a DVI-D port or built in LCD expansion connector. In addition to this, the flexible, USB-enabled expansion allows users to start developing quickly using their existing PC's USB peripherals. The expansion header allows them to leverage Parallel Flash Bus, MMC, SPI and I2C for greater development potential.
PTM Veröffentlicht am: