Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
Channel Link Slide 13

Shown here is the need for signal conditioning with long reaches of cable. The first line is the waveform starting at the source (TP1), after the cable (TP2) and after a buffer with no EQ. As shown in the waveform, there is a lot of jitter and not great quality. When signal conditioning is used at the transmit stage as shown in line two, the waveform at the end of the cable (TP2) is better. After applying an equalizer, the jitter is vastly reduced and signal quality is good.

PTM Veröffentlicht am: