Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Analog Switch Solutions Slide 5

The TS5A3153 is a single-pole double-throw (SPDT) analog switch that is designed to operate from 1.65 V to 5.5 V. This switch has the capability to mute the audio signal or select the speaker output. The device offers a low ON-state resistance and an excellent ON-resistance matching with a break-before-make feature, to prevent signal distortion during the transfer of a signal from one channel to another. The TS5A3153 has excellent total harmonic distortion (THD) performance and consumes very low power.

PTM Veröffentlicht am: