Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
CLL-Slide5

The CLL Series is designed for high speed applications such as a Central Processing Unit and a Graphics Processing Unit. The diagram shown here is an evaluation result on the Low ESL effect. In the IC power line shown, the voltage drop is due to current fluctuations that occur when the power is turned on. Voltage drop can be reduced by lowering the ESL, making the Ultra Low Inductance capacitor series an excellent choice for applications that operate at higher frequencies.

PTM Veröffentlicht am: