Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
Closed-Loop Hall Effect Sensors Slide 8

Closed loop Hall Effect current sensor specifications define the input current as the rated, primary, or nominal current rating of the sensor as a DC or RMS current. The output or secondary current is rated in instantaneous current, in either DC or AC. The output current tracks the input current exactly, there is no RMS conversion made by the current sensor.

PTM Veröffentlicht am: