Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
TI900 Silicone Based Thermally Conductive Insulators Slide 6

When using an insulator, such as TI 900, one of the key design parameters is the dielectric breakdown voltage. This is a measure of how well a material can prevent the voltage from the component case from arcing through the material and creating an electrical short circuit. The higher the dielectric breakdown voltage, the better the material’s performance is deemed to be. This is tested with reference to ASTM D149.

PTM Veröffentlicht am: