Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
TG-CPCB Ceramic PCBs Slide 4

IMS (Insulated Metal Substrate) boards, also sometimes known as Metal Core PCB (MCPCB) consist of a metal base plate, a thin dielectric layer, and a layer of copper to be used to lower thermal resistance. The dielectric is normally 100 microns as it is a poor thermal conductor. The metal plate is then screwed to a heatsink using a thermal interface such as a grease of a silicone base pad. IMS can provide effective thermal management but issues remain over its reliability.

PTM Veröffentlicht am: