Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
Heat Spreading Solutions for TV Applications Slide 11

The data presented above is taken from a real TV application which is in full-scale mass production. Both the XLi98(C) and the XL25 (minus the thermal tape) passed the stringent dielectric breakdown voltage tests required for consumer electronic production. This is important to the industry and gives the designer a greater degree of flexibility. improved performance, and reliability.

PTM Veröffentlicht am: