Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Intelligent Power Switches Slide 9

Even in the event of a short circuit between the output of the IPS and the ground, the current will be limited without damaging the silicon. This is maybe the most important feature and differentiation with automotive IPS. If the current limit is too high, this can destroy the load and even burn the board. Typically, for a standard current of 0.7 A, the current limit will be slightly more than 1 A. In addition, for a standard current of 1 A, the current limit is roughly 1.5 A. An optimized current limit is also very important for good thermal management. Indeed, a high current will increase the temperature in the package and the thermal shut down will be reached faster.

PTM Veröffentlicht am: