Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
Intelligent Power Switches Slide 5

Another way to find opportunities for the IPS is to ask customers if they use relays. The IPS can in fact replace the relays. The advantage of an IPS Versus a relay is reliability. The other advantages are the space and all the protection and diagnostic features that a relay cannot implement. A summary of these features are presented next slide.

PTM Veröffentlicht am: