Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Bluetooth Modules and Turnkey Solutions Slide 5
The Bluetooth system partitioning realized by ST Blue modules is the integrated or embedded solution. This means that all the Bluetooth firmware from the stack to the profile set, including driver and interface applications are embedded in ST modules. The only external component required is the application processor driving in the final application system. This approach overcomes the RF integration issue in the final application and confines the Bluetooth certification to the module. Little effort is required to integrate an ST Blue module in the final application.
PTM Veröffentlicht am: