Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
AC Switches Family - Part 2 Slide 4

This slide shows another typical application for run and start inside of a compressor.  In these types of applications with inductive motors, it is very good to have high-immunity dV/dt against fast voltage transients and to have overvoltage clamping devices. This feature is built into the ACST and an external clamping device is not required.

PTM Veröffentlicht am: