Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
AC Switches Family - Part 2 Slide 2

Shown on this slide is an example of the use of TRIACs. There are several used in this system, some have resistive loads and some have motors. They are direct driven by a microcontroller with a resistor in series with the gate. As can be seen, when using a sensitive gate TRIAC the circuit can have energy savings because the trigger current is low, therefore the current needed from the microcontroller is low.

PTM Veröffentlicht am: