Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
auto-liquid-slide4

The sensing distance for a given application may be adjusted for optimum closing and opening to best suit the application. Here the sensitivity of closure is measured in milliTesla or ampere turns. This is called the pull-in point.  Removing the magnet, the contacts will open at some point. This is called the drop-out point. Hysteresis is another useful parameter and can be adjusted to optimize a given application. Hysteresis is simply the ratio of the closure distance divided by the opening distance. The hysteresis can be critical for some applications. 

PTM Veröffentlicht am: