Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Inno Arch

The isolation technology used on the Si87xx is based on patented inventions. The block diagram on this slide shows the components for the isolation signal path. The isolation provides a withstand rating of 5 kVrms. Skyworks Solutions isolation is purely CMOS based and uses silicon dioxide as a dielectric. Silicon dioxide is highly effective in this capacity because of its wide availability, high intrinsic breakdown of >500 V/µm and resistance to environmental factors. Signals cross the isolation barrier through a pair of differential capacitors. The differential signaling, along with the small size of the capacitors, ensures that the isolation achieves good EMI and reduces emissions. Low input to output parasitic capacitance means that the devices have high common mode immunity. The Si87xx isolation fully meets the requirements for reinforced IEC60747-5-2 certification, including protection from surges up to 10 kV.

PTM Veröffentlicht am: