Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
hi perf on class
The RX family offers highest performance in class with the RX core running at up to 240 MHz with 4.55 CoreMark per MHz. Up to 4 MB of Flash makes RX the MCU in the market with one of the largest Flash. The Flash runs at up to 120 MHz, enabling Zero-Wait states for unlimited performance. Broad connectivity and unique features are showing the power of these devices.
PTM Veröffentlicht am: