Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
PLL LO Gen

As described previously, the TFF1003 is the basis of a full family of LO generators by NXP. These LO generators can by used for multiple applications in the Transmit (Tx) or Receive (Rx) chain. Here is an overview of all the types that NXP has developed so far. The types in green are released and the types in yellow are available as samples and will be released in the near future. The RF performance of the TFF11xxx-family is roughly the same as the TFF1003, only the VCO frequency is different for each type.

PTM Veröffentlicht am: